Surgical tool tracking with RFID

With RFID technology Murata supports
the improvement of safety and efficiency during surgery.

US regulations require a UDI (Unique Device Identifier)* be placed on each surgical tool by 2020. Europe follows this movement and plans to complete by 2027.
Additionally, the set up of surgical tools is time consuming even by highly skilled and experienced operators. How to make the process more efficient is a big challenge.

* UDI(Unique Device Identification) regulation
The rule of a product identification that should be applied to all medical devices for the safe use and storage.

Difficulties in surgical tool market

  • Image showing how the ID is applied to each instrument

    • Worldwide trend to make it compulsory to put ID on each surgical tool.
  • Image showing the challenges of tracking surgical instruments

    • Cannot accurately manage use time due to the difficulty with using manual records.
      Assembling and checking the set of tools takes time and manpower.
  • The illustration of how difficult it is to read barcode on surgical instrument

    • Laser marking is vulnerable to rust and stain.
    • 1by1 reading of ID from QR code is time consuming.

Advantages of RFID

Image showing how the RFID is applied to surgical instruments. Various information can be written and read inside.

  • RFID tag as unique ID.
  • Record of use time and life time, makes management easier.

The illustration of mass reading of surgical instruments with hand held reader

  • Quick and batch reading with RFID enables operators to efficiently assemble and check the set of tools.

The usage frequency of the surgical instruments will be recorded in the data. It can be displayed on PC's and other devices.

  • Measuring the times of use for each tool to reduce excessive amount of stock.
  • Recording the order of the use to optimize the preparation of tools before surgery.

Why RFID

  • Efficient Inventory count and time usage management.
  • Reading in batches for quick management.
  • Reading is possible even when covered with blood after surgery.

Why Murata

  • RFID tag for on-metal application is available.
  • Robust RFID tag that can survive auto-clave process is available.
  • Murata can offer support on the reading environment and how/where to attach the tag with in-depth knowledge on RF technology.

Reading method

  • The illustration of mass reading of surgical instruments with hand held reader

    • Scanning with hand-held reader writer.
  • Real time reading of all surgical instruments on the table with fixed reader and antenna

    • Set reader writer and antennas to read tags without manual operation.

Read range (Reference)

  • 10cm~1m
    * Read range is subject to change upon the evaluated environment.

For customers looking for RFID tag/reader-writer.

Murata also offers hardwares from the lineup of RFID tag and reader-writer. Please find the detail in the product page.