Ayla IoT Platform

Overview

The IoT Platform for the World's Leading Manufacturers

Built for enterprise-scale, Ayla's Agile IoT Platform was architected from the ground up to deliver a truly end-to-end software foundation that would enable any device manufacturer to develop elegant and reliable connected products.

Comprised of three primary components - Ayla Embedded Agents, Ayla Cloud Services, and Ayla Mobile SDKs - Ayla's Agile IoT Platform provides a complete, end-to-end solution that connects nearly any device to the cloud and applications while offering all of the tools and premium services needed for a manufacturer to provide, manage, and analyze their Internet of Things deployment. Ayla empowers leading manufacturers by solving the inherent complexities of the IoT so they can focus their resources on where it matters.

For more information, visit https://www.aylanetworks.com/products/iot-platformOpen in a new window

Ayla's Agile IoT Platform™

Features

Platform Component: Device

Drop-in Networking

Pre-programmed, fully tested, and production ready hardware

Industry Standard Hardware

Support for industry leading, "Off-the-Shelf" hardware

Broadest Support

Support for embedded & Linux based applications to cover the broadest array of communication protocols and use cases

No Additional Cost

Ayla's Embedded Agent adds ZERO additional cost to hardware

Platform Component: Device

Platform Component: Cloud

Highly Scalable

Ayla's Cloud operates atop the global AWS infrastructure

Unmatched Flexibility

No fixed data schema & support of RESTful APIs

Configuration over Coding

Ayla's Cloud requires zero "cloud" coding for customers

Enterprise Security

Enterprise class security with multi-layer authentication and access controls

Out-of-the-Box

Support for device & user management, notifications, data management, and other services and features, day one

Platform Component: Device

Platform Component: Applications

Mobile SDKs

Native Android (Java) and iOS libraries (Objective- C and Swift)

Defined Logic

Mobile libraries support creation of triggers, schedule, timers, registration, and account CRUD

LANConnect

Local communication to maintain device connectivity in the event of a loss of broadband in the WLAN

AMAP

Partially configured mobile application to speed application development and lower costs

Platform Component: Applications

Focus: SCALABILITY & SECURITY

Standard

Ayla has ISO 27001 and SOC2Open in a new window

LANConnect

Secure peer-to-peer connection between mobile apps and IoT devices when on the same WLAN

TLS 1.2 Encryption

Protects user privacy as customer data and key information is never exposed, end-to-end

Root Key Protection

Device keys, burned into connectivity modules at factory, are never exposed

Multi-Layer Authentication

Cloud enforces authentication of device, app, and user to ensure integrity and protect against piracy

Elastic Cloud Computing

Ayla can dynamically scale to your business, data flow, and analytical load, no matter how fast you grow

Global Cloud Footprint

Cloud operations across Asia, Americas, and Europe to accommodate your global business

Focus: LEVERAGE YOUR DATA

Device Virtualization

Virtual device definitions maintained in the cloud, separate from data schema to easily support device changes

Data Visualization

Use Ayla's built-in reporting and visualization tools to see and use your collected data with self-service business intelligence

IoT Analytics

Import/export data with practically any 3rd party to expand functionality and application integration

Ayla Insights

Fully integrated business intelligence and analytics platform that provides real-world insights into how your connected products are being used

Focus: LEVERAGE YOUR DATA

AYLA's CORE VALUES

Ayla Solves the Internet of Things so You Don't Have To

  • End-to-end configurability for fastest time to market
  • Flexibility to learn & adapt on the go
  • Enterprise security & scalability
  • Unmatched quality & reliability
  • Global coverage
  • Fastest path to leverage your data
Simple interface is cool

Contact us:
https://www.aylanetworks.com/company/contact-usOpen in a new window

*We do not sell "Ayla IoT Platform" as a finished product. This is just an example of how Murata products are used in actual applications.

Contact

Please make inquiries about our solutions introduced here using the contact form below.


Partner Collaboration Solutions

Connectivity Solutions For NVIDIA🄬 JETSON™

Murata provides wireless connectivity solution to realize easy integration for NVDIA🄬 JETSON™ Nvidia's strong AI platform and Murata's wireless solution offer easy solution to achieve time to market.

Wi-Fi ® sensing for child presence detection(CPD)

Wi-Fi sensing can accurately detect breathing and motion anywhere inside the car without blind spots. Wi-Fi sensing can be freely located in contrast to cameras.

Murata’s Wi-Fi®/Bluetooth® and Cellular Cat-M1/NB-IoT AWS qualified modules enable cloud-connected IoT devices

Murata's qualified connectivity modules combining the excellence in module manufacturing with a large and diversified products portfolio, together with AWS cloud excellence powered by over 175 services and a dedicated IoT Core platform - providing scalability, security, analytics and device management services, accelerate and simplify the journey to develop IoT devices and end-to-end solutions.

Accelerating the AI & IOT solutions enriching our lives

Google combined Murata’s compact package technology and Google’s own Edge TPU chip enabling power-efficient and high-performance machine learning inference to create a new compact AI module.

VitaNet and Murata join forces to utilize Murata Bluetooth® module with QR code to convert industrial components to IoT

Cloud is enabled to directly control Bluetooth® device by reading QR code to identify a device. Authentication and secure Bluetooth® communication follow automatically.

Electric Imp IoT Connectivity Platform

Innovative platform which simply connects devices and the cloud

LPWA/Bluetooth® Low Energy Tag Linking Solution

"Condition" and "status" management solution utilizing LPWA

Integrated Wi-Fi+Bluetooth® MCU Modules

Integrated Wi-Fi, Bluetooth communication function and micro control unit in a single unit Easy to Use AT Command (Serial Communication)

Ayla IoT Platform

Ayla's end-to-end IoT software applications to provide secure and scalable connectivity, data analytics, and seamless user experiences. Ayla is solving the IoT so you don't have to.