Description
Partners that can collaborate with us to create unique products by utilizing ultra-thin, high sensitivity film thermistors
Products used
Sheet-shaped temperature sensors called film thermistors that have a thickness of just 50 microns and can be freely bent
*This product is under development.Therefore, the product specifications are subject to change without advance notice.
MATCHING
POINT

In order to obtain the maximum performance from electronic devices such as PCs and smartphones, and to help prevent accidents, accurate temperature measurement of batteries and other components is essential. For this reason, Murata Manufacturing has developed an ultra-thin sheet-shaped temperature sensor called a film thermistor. This film thermistor is highly sensitive and has a fast response speed, allowing it to quickly capture changes such as slight temperature variations and sudden rises in temperature. It is also thin and can be freely bent, which enables insertion into thin gaps to measure temperature. Furthermore, multiple film thermistors can be arranged side-by-side to understand temperature distributions. We are looking for co-creation partners that want to solve challenges by utilizing this film thermistor in new product development and thermal analysis.
An ultra-thin thermistor is formed on resin film.
A film thermistor is a sheet-shaped NTC thermistor capable of temperature measurement. Murata has succeeded in forming an ultra-thin thermistor on resin film.
The core of this technology is low-temperature ceramic sintering technology, and original Murata technology developed over many years of ceramics R&D, as well as sheet-related technology for board products, is also utilized. This film thermistor can be considered the crystallization of Murata’s technology.
Here is a demonstration video introducing the film thermistor shape and response speed, as well as the transition of heat through multi-point detection. Please take a look.
While conventional chip thermistors have a thickness of around 300 microns (assuming 0402 size), the film thermistor achieves a thickness of 50 microns, which is just 1/6 of that. Furthermore, the use of technology for sintering ceramics at low temperatures has made it possible to form an ultra-thin thermistor on resin film. The thinner shape gives the film thermistor features not available with conventional chip thermistors (for more details, see Feature 02 below).
Achieves a thickness of 50 microns, The film thermistor is extremely thin, which results in a smaller heat capacity compared to conventional chip thermistors, making it possible to detect extremely small temperature changes. It also features a fast response speed that enables swift tracking and accurate measurement of even sudden temperature changes in the measured object.
Because the sensor is so thin, it picks up even the most subtle temperature variation.
Because the sensor is so thin, it immediately measures any sudden thermal variation.
The film thermistor can be bent up to a radius of 1 cm. This characteristic enables to wrap it around objects such as pipes or plants, or attach it to complex curved surfaces to measure their surface temperatures. Because the film thermistor is thin and can be freely bent, it can accurately measure temperature in narrow gaps and other locations that were a challenge with conventional chip thermistors. In addition, the film thermistor also has high pressure resistance, enabling temperature measurement in locations subject to pressure.
The film thermistor is flexible and can be bent up to a diameter of 1 cm.
Use of multiple film thermistors arranged in a planar configuration makes it possible to measure temperature distributions and visualize the flow of heat. This enables measurement of temperatures in hidden areas that cannot be captured by thermography.
The “flow of heat” can be captured by arranging multiple film thermistors side-by-side.
Monitoring battery temperature to detect degradation and signs of danger
Use is expected for temperature monitoring of batteries in smartphones, laptop PCs, electric vehicles, and so on. Detailed temperature control will enable early detection of degradation and signs of danger, and make it possible to enhance battery performance and to extend the operating time of devices and the driving range of electric vehicles.
Mounting in masks, etc. to understand changes in body temperature
Applications that make use of the thin-film shape are expected in the health and medical device field. For example, mounting film thermistors in masks, etc. to measure body temperature will help to understand health status, and may assist in diagnosis and disease prevention. Other applications include attachment to the tip of an endoscope to conduct real-time measurement of internal body temperature for diagnostic purposes, and use in the development of accurate thermometers that work in a shorter time.
Contributing to increasing production process stability and improving quality
Thermal design of factory production equipment and electronic devices faces many challenges such as the complexity of temperature control, heat generation countermeasures, and cost constraints. By leveraging the features of film thermistors such as a fast response speed and multi-point measurement, the flow of heat can be visualized in real time, greatly contributing to increasing the stability of production processes and improving quality.
Murata Manufacturing is looking for co-creation partners who seek to develop new products that utilize film thermistors or to use film thermistors in thermal analysis to solve challenges.
If your company is interested in collaborating with Murata Manufacturing, please feel free to contact us using the Inquiry form.
*This product is under development.Therefore, the product specifications are subject to change without advance notice.
Murata Manufacturing Co., Ltd.
Advanced Technologies Research & Development Department, New Technologies Center, Corporate Technology & Business Development Unit
Miniaturization and higher performance of electronic devices have led to a rapid increase in heat-related challenges. We want to transcend industry boundaries and work together with companies facing challenges with conventional temperature measurement methods to create as many innovations as possible. Please feel free to contact us.
At an exhibition where we showed the film thermistor, the positive reactions from visitors reaffirmed that this is a technology that can contribute to society. We feel great potential in this technology that enables real-time monitoring of areas and temperature fluctuations that are a challenge to measure by conventional methods. Going forward, it would make us happy to be able to expand the range of objects that can be temperature-controlled and make contributions in various fields.
My career has been one with this technology ever since being assigned to research and development of film thermistors upon joining Murata. We take pride in the film thermistor, which was born from pursuing extreme thinness, as a technology overflowing with Murata’s unique style. Just as Murata has provided value to the world through pursuit of miniaturization, we believe this product can also offer new value through “thinness.”

Murata Manufacturing is looking for co-creation partners who seek to develop new products that utilize film thermistors or to use film thermistors in thermal analysis to solve challenges.
If your company is interested in collaborating with Murata Manufacturing, please feel free to contact us using the Inquiry form.
*This product is under development.Therefore, the product specifications are subject to change without advance notice.