Enter a product part number, or a portion of a part number.

Effortlessly and securely connect your smart devices leveraging Cellular IoT technology and LwM2M Protocol with Murata, ST and AVSystem End-to-End solution
[Cellular IoT Technology + LwM2M Protocol]
End-to-End Solution


LTE Cat. M1 is a licensed standard that requires a license to use the radio frequency band. It is ideal for cases whereby IoT needs to minimize costs and power consumption even if speeds are slow. LTE Cat. M1 is particularly suitable for mobile communications, such as when devices are moving, and because it uses licensed bands, radio interference is less likely to occur, and speeds are faster, allowing it to be used for wearable devices in IoT and other applications.
"NB" is an abbreviation for "Narrow Band." These modules can easily run on less power than LTE modules. These modules are expected to be used for IoT solutions that require low power consumption, and are suitable for environments where batteries are not easily replaceable or where a commercial power supply is unavailable, such as smart meters and other remote medical examinations, crop growth management, alarm notifications for security devices, and detection of anomalies when disasters occur. They are also expected to be used for predictive maintenance of public infrastructure and similar applications.
Flick scroll

To learn more:

Lightweight M2M (LwM2M) is a standard created by OMA SpecWorks in 2017 that specifies device management, telemetry and service enablement mechanisms designed initially for devices that have limited processing and storage capabilities (commonly referred to as resource constrained devices). It is based on UDP/TCP data transport protocols and uses a standardized data mode to exchange of information between device and platform divided into three object levels: Object, Object Instance and Resource. Each object is assigned a unique ID, which is then combined to form a path and a CoAP URL.
The technology functions very well over potentially unstable and low bandwidth networks such as cellular as well as LPWA radio networks. Besides LwM2M protocol helps to minimize the energy related to the initial connection and data transport, allowing to increase battery life for battery operated IoT devices, providing a single-step commissioning and easy bootstrapping. It can also be used for device management such as over-the-air update, as well as offers lightweight security options such as Oscore.
To learn more:

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata website
.
At ST, we are 46,000 creators and makers of semiconductor technologies mastering the semiconductor supply chain with state-of-the-art manufacturing facilities. An independent device manufacturer, we work with more than 100,000 customers and thousands of partners to design and build products, solutions, and ecosystems that address their challenges and opportunities, and the need to support a more sustainable world. Our technologies enable smarter mobility, more efficient power and energy management, and the wide-scale deployment of the Internet of Things and 5G technology. Further information can be found on STMicroelectronics website
.
AVSystem is a vendor of Internet of Things and device management software present on the market since 2006. Our mission is to develop solutions that help enterprises create and manage ecosystems of connected devices. We offer platforms for device and network management, IoT application enablement, WiFi marketing and indoor location, as well as embedded tools. As market leaders in IoT device management, we manage millions of devices worldwide. We focus on scalable solutions based on standards such as LwM2M to help companies speed up the time to market of their IoT projects. Visit AVSystem website
for more information.
Murata's lineup includes two LTE Cat-M1 and NB-IoT modules to easily bring cellular connectivity to your smart IoT device and scale your deployment globally.
"All-in-One" module includes Type 1SC packaged with STMicro STM32L4 MCU and ST4SIM GSMA-certified eSIM. It is certified globally with the MVNO Truphone, bringing seamless connectivity in over 100 countries and includes a U.FL connector to just plug the antenna.
A standalone modem based on Sony ALT1250 SoC and certified with Tier1 cellular network operators globally. It also supports GNSS (GPS, Glonass) & Polte for geolocation, OpenMCU and an integrated SIM (iSIM) as options.

Type 1SE
The LBAD00ZZ1SE module is a dual-mode Cat. M1/NB-IoT module with built-in MCU from STMicro, MVNO-compatible eSIM, and antenna connector. It supports various certifications and is suitable for speeding up the development process.

Type 1SC
The LBAD00XX1SC module is the world's smallest Cat. M1/NB-IoT module with global certification. It supports GPS/GNSS, OpenMCU, Integrated SIM.
Type 1SE is recommended for quicker Time-to-Market, simplifying both the HW and SW design with a guarantee of best performances. Indeed, main effort will be the Application development greatly simplified by the Software Development Kit (SDK) called X-CUBE-CELLULAR provided by ST. Learn more![]()
Type 1SC allows design customization, such as the selection of a specific external host MCU, or to leverage features such as geolocation, iSIM, etc. The mode of operation by default is to use an external host MCU by sending AT commands. However, it is also possible as an option to utilize the X-CUBE-CELLULAR SDK with an external host MCU from ST in order to simplify Application development.
Flick scroll

Both "Hostless" and "Hosted" design options are available to offer flexibility to define most suitable architecture for End Device requirements.
Flick scroll

Murata Type 1SE module, in collaboration with STMicro and AVSystem, can be leveraged to develop complete End-to-End IoT Solutions, speeding up time to market.
Flick scroll

The solution utilises STMicro's X-CUBE-CELLULAR SDK and AVSystem's Anjay L2M2M Client SDK and Coiote IoT Device Management (DM) Platform to perform over-the-air update or access 3rd party cloud platform such as AWS or Azure.
Flick scroll

To use AVSystem 's Coiote IoT DM platform, you need to create a new user account first.
Click on the following link to sign up for free trial account here ![]()
Flick scroll

To manage your devices over AWS, LwM2M operations can be performed from either Coiote DM side or AWS IoT side using the Operation Shadow in Device Shadows. Check this link
to view an example on how to perform operations like READ, WRITE , OBSERVE, EXECUTE.
READ Request
Flick scroll

To integrate with Microsoft Azure, note that users can choose to provision and synchronise their devices to either Azure IoT Hub or Azure IoT Hub with Device Provisioning Service (DPS) or Azure IoT Central.
How are they different? IoT Central is a fully managed (aPaaS) with ready made templates and services, for organisations to build their IoT solutions. On the other hand, IoT Hub (PaaS) is geared towards developers who want to customise and build their own IoT solution from scratch.
What about Azure DPS?
Azure IoT Hub Device Provisioning Service (DPS) is a helper service for Azure IoT Hub that enables zero-touch provisioning of IoT devices at scale. Azure DPS ensures high availability by providing load balancing across multiple hubs and supporting reprovisioning based on a change in the device. For more information about Azure DPS, refer to the official documentation.
How to integrate Azure IoT Hub (and use DPS)?
Flick scroll

To integrate with Azure IoT Central:
The I-CUBE-Anjay LwM2M Client SDK (I-CUBE-Anjay) allows user to perform application software over-the-air-update by leveraging ST X-CUBE-SBSFU function embedded in the SDK.
Please follow the instructions in this GitHub repository to try the OTA demo.
Process for Type 1SE:
Use the X-CUBE-SBSFU to download a new image from the LwM2M server into the 1MB on-board Serial Flash in 1SE module, then install the new image into the internal STM32L462 MCU 512KB Flash.
Flick scroll

Steps:
To learn more:
To contact ST or AVSystem:
All About Murata C-IoT Products and Solutions
Please make inquiries about our solutions introduced here using the contact form below.
End-to-End cellular IoT solution from Murata × ST × AVSystem
Leveraging on Murata’s LTE Cat-M1 and NB-IoT modules; STMicro's X-CUBE-CELLULAR SDK; and AVSystem's Anjay L2M2M Client SDK and Coiote IoT Device Management (DM) Platform, this end-to-end solution enables effortless and secure connection for your smart IoT devices.
Connectivity Solutions For NVIDIA🄬 JETSON™
Murata provides wireless connectivity solution to realize easy integration for NVDIA🄬 JETSON™ Nvidia's strong AI platform and Murata's wireless solution offer easy solution to achieve time to market.
Murata’s certified module on Everynet LoRaWAN® network operated by Telkom Indonesia change the dynamics of Industrial Revolution 4.0 to enable millions of connected IoT devices
Murata provides designers with a turn-key LoRaWAN® connectivity module solution to simplify and accelerate their IoT products development together with Everynet, a global leading LoRaWAN® network operator and Telkom Indonesia, the largest telecommunication and network provider in Indonesia, to enable the deployment of secure end-to-end solutions to address multiple applications in the smart cities, utilities, logistics and tracking, agriculture and many others.
Wi-Fi ® sensing for child presence detection(CPD)
Wi-Fi sensing can accurately detect breathing and motion anywhere inside the car without blind spots. Wi-Fi sensing can be freely located in contrast to cameras.
Murata’s Wi-Fi®/Bluetooth® and Cellular Cat-M1/NB-IoT AWS qualified modules enable cloud-connected IoT devices
Murata's qualified connectivity modules combining the excellence in module manufacturing with a large and diversified products portfolio, together with AWS cloud excellence powered by over 175 services and a dedicated IoT Core platform - providing scalability, security, analytics and device management services, accelerate and simplify the journey to develop IoT devices and end-to-end solutions.
Accelerating the AI & IOT solutions enriching our lives
Google combined Murata’s compact package technology and Google’s own Edge TPU chip enabling power-efficient and high-performance machine learning inference to create a new compact AI module.
VitaNet and Murata join forces to utilize Murata Bluetooth® module with QR code to convert industrial components to IoT
Cloud is enabled to directly control Bluetooth® device by reading QR code to identify a device. Authentication and secure Bluetooth® communication follow automatically.
Electric Imp IoT Connectivity Platform
Innovative platform which simply connects devices and the cloud
LPWA/Bluetooth® Low Energy Tag Linking Solution
"Condition" and "status" management solution utilizing LPWA
Integrated Wi-Fi+Bluetooth® MCU Modules
Integrated Wi-Fi, Bluetooth communication function and micro control unit in a single unit Easy to Use AT Command (Serial Communication)
Ayla IoT Platform
Ayla's end-to-end IoT software applications to provide secure and scalable connectivity, data analytics, and seamless user experiences. Ayla is solving the IoT so you don't have to.