Built for enterprise-scale, Ayla's Agile IoT Platform was architected from the ground up to deliver a truly end-to-end software foundation that would enable any device manufacturer to develop elegant and reliable connected products.
Comprised of three primary components - Ayla Embedded Agents, Ayla Cloud Services, and Ayla Mobile SDKs - Ayla's Agile IoT Platform provides a complete, end-to-end solution that connects nearly any device to the cloud and applications while offering all of the tools and premium services needed for a manufacturer to provide, manage, and analyze their Internet of Things deployment. Ayla empowers leading manufacturers by solving the inherent complexities of the IoT so they can focus their resources on where it matters.
For more information, visit https://www.aylanetworks.com/products/iot-platform
Pre-programmed, fully tested, and production ready hardware
Support for industry leading, "Off-the-Shelf" hardware
Support for embedded & Linux based applications to cover the broadest array of communication protocols and use cases
Ayla's Embedded Agent adds ZERO additional cost to hardware
Ayla's Cloud operates atop the global AWS infrastructure
No fixed data schema & support of RESTful APIs
Ayla's Cloud requires zero "cloud" coding for customers
Enterprise class security with multi-layer authentication and access controls
Support for device & user management, notifications, data management, and other services and features, day one
Native Android (Java) and iOS libraries (Objective- C and Swift)
Mobile libraries support creation of triggers, schedule, timers, registration, and account CRUD
Local communication to maintain device connectivity in the event of a loss of broadband in the WLAN
Partially configured mobile application to speed application development and lower costs
Secure peer-to-peer connection between mobile apps and IoT devices when on the same WLAN
Protects user privacy as customer data and key information is never exposed, end-to-end
Device keys, burned into connectivity modules at factory, are never exposed
Cloud enforces authentication of device, app, and user to ensure integrity and protect against piracy
Ayla can dynamically scale to your business, data flow, and analytical load, no matter how fast you grow
Cloud operations across Asia, Americas, and Europe to accommodate your global business
Virtual device definitions maintained in the cloud, separate from data schema to easily support device changes
Use Ayla's built-in reporting and visualization tools to see and use your collected data with self-service business intelligence
Import/export data with practically any 3rd party to expand functionality and application integration
Fully integrated business intelligence and analytics platform that provides real-world insights into how your connected products are being used
*We do not sell "Ayla IoT Platform" as a finished product. This is just an example of how Murata products are used in actual applications.
Please make inquiries about our solutions introduced here using the contact form below.
Wi-Fi ® sensing for child presence detection(CPD)
Wi-Fi sensing can accurately detect breathing and motion anywhere inside the car without blind spots. Wi-Fi sensing can be freely located in contrast to cameras.
Murata’s Wi-Fi®/Bluetooth® and Cellular Cat-M1/NB-IoT AWS qualified modules enable cloud-connected IoT devices
Murata's qualified connectivity modules combining the excellence in module manufacturing with a large and diversified products portfolio, together with AWS cloud excellence powered by over 175 services and a dedicated IoT Core platform - providing scalability, security, analytics and device management services, accelerate and simplify the journey to develop IoT devices and end-to-end solutions.
Accelerating the AI & IOT solutions enriching our lives
Google combined Murata’s compact package technology and Google’s own Edge TPU chip enabling power-efficient and high-performance machine learning inference to create a new compact AI module.
VitaNet and Murata join forces to utilize Murata Bluetooth® module with QR code to convert industrial components to IoT
Cloud is enabled to directly control Bluetooth® device by reading QR code to identify a device. Authentication and secure Bluetooth® communication follow automatically.