Murata’s certified module on Everynet LoRaWAN® network operated by Telkom Indonesia change the dynamics of Industrial Revolution 4.0 to enable millions of connected IoT devices

Overview

Why LoRaWAN™?

LoRa Alliance

LoRaWANTM is a standard developed by the non-profit organization LoRa AllianceTM. LoRa AllianceTM members include many IoT companies from around the world. LoRaWANTM uses the unlicensed band signals of the sub-gigahertz band that does not require a license (around 900 MHz. 920 MHz in Indonesia), and its maximum packet size is 256 bytes and its speed is 200 to 10 kbps. An additional feature is that its high noise immunity makes it highly sensitive to radio waves from devices connected to a wireless network.

This enables LoRaWANTM to act as a specialized long-range technology to send and receive data not only in urban areas, but also in mountainous areas and on remote islands.
Murata's Low Power Wide Area (LPWA) wireless modules are the industry's smallest modules, enabling the design of a wide range of compact end devices.
*LoRaWANTM is certified by the LoRa AllianceTM.

To learn more: LoRa (LoRaWAN) ModulesOpen in a new window

Why Telkom-Everynet?

Telkom IoT by Telkom Indonesia-Everynet

Telkom Indonesia, Indonesia's largest telecommunication and network provider, and Everynet BV, a global LoRaWAN network operator and provides carrier grade networks in Asia, EMEA, and the Americas, have partnered to build-out, operate and accelerate the expansion of national LoRaWAN IoT network infrastructure to enable the Industrial Revolution 4.0 in Indonesia. They are committed to building and developing a National Digital Platform that all industry players including startups can use. Services include the use of Data Centers, Big Data, Internet of Things (IoT), Artificial Intelligence, Cloud, Security and Payment/Blockchain. This initiative is expected to support the government in accelerating the digital economy, as well as supporting industry 4.0..

The Telkom-Everynet joint venture will enable all of Indonesia’s MNOs, ASPs, MSPs & ISPs to offer robust Low-Power Wide-Area (LPWA) IoT services, with the lowest shared costs and the shortest time to revenue. IoT services will allow end users to gather huge amount of previously ignored data, which will help to take informed and real-time decisions on many aspects of Indonesia economic and social life.

To learn more: Telkom IOTOpen in a new window

Why Murata LoRa (LoRaWAN) modules?

Murata, the largest connectivity modules manufacturer in the world, is a member of the LoRa Alliance™ and has worked with STMicro and Semtech to design a low-cost, compact LoRaWAN™ module that supports a variety of sensors and long-range wireless protocols.

Murata's LoRa (LoRaWAN) modules are pre-certified in accordance with the Radio Law to operate in the 800-900 MHz Industrial, Scientific and Medical (ISM) band and can operate in many regions of the world. The LoRa platform provides hardware and software for this fully-verified module.

To learn more: LoRa (LoRaWAN) ModulesOpen in a new window

Solution

What is Everynet certification?

Everynet E-thingz certified

Everynet certification allows partners like Murata to validate that their devices interoperate with Everynet's neutral-host IoT infrastructure, implement best practices, and giving OEMs and their customers the confidence that devices interoperate correctly and consistently. Qualification is based on the technical validation of LoRaWAN stack implementation, and operation on the Telkom LoRaWAN network.

About Everynet BV

The Global Leader in Neutral Host, Ultra Low Cost IoT Connectivity
Everynet BV is a global LoRaWAN network operator and provides carrier grade networks in Asia, EMEA, and the Americas. Everynet’s Neutral Host network model enables Mobile Network Operators, MVNO’s, and Global MSP’s to offer ultra-low cost IoT immediately and profitably with ZERO upfront CAPEX. Everynet makes IoT accessible across any industry to enable enterprise-grade solutions and is deployed using LoRaWAN technology, the globally adopted open standard for IoT connectivity.
For more information, please visit hereOpen in a new window.

Murata’s Everynet certifed LoRa (LoRaWAN) modules currently include Type 1SJ:

LBAA0QB1SJ

Type 1SJ

The LBAA0QB1SJ module is one of the smallest LoRaWAN™ modules in the industry. This module has a lower power consumption and higher output than previous products. Radio Law certification has already been obtained for major regions.

Detailed SpecificationsOpen in a new window

CMWX1ZZABZ

Type ABZ

The CMWX1ZZABZ module is a LoRaWAN™ module that operates in many regions and operator networks around the world. Radio Law certification has already been obtained for major regions.
This module can also support Sigfox by modifying the software.

Detailed SpecificationsOpen in a new window

Compelling Value Proposition for IoT Devices

Leverage respective companies unique strength to ease and speed up the journey to develop your IoT device using Telkom's LoRaWAN and Antares platform, and Murata's certifed modules.

Flick scroll

Antares is Telkom's IoT platform to securely connect devices to the cloud & other devices, secure data and interactions, process and act upon it.

Flick scroll

Example of Applications using LoRaWAN:

Flick scroll

Video 1: Summary of 1SJ EVK connection bring-up on Telkom Antares platform

Note: this video is also available on YoutubeOpen in a new window.

Enabling captions is quick and easy.

  1. Tap the three-dot menu (*upper right corner)
  2. Tap the CC (Captions) icon in the menu
  3. Select your captions preferences

Video 2: ABZ EVK connection bring-up on Telkom Antares platform

Note: this video is also available on YoutubeOpen in a new window (in Bahasa Indonesia).

Enabling captions is quick and easy.

  1. Tap the three-dot menu (*upper right corner)
  2. Tap the CC (Captions) icon in the menu
  3. Select your captions preferences

To learn more:
Telkom IOTOpen in a new window
EverynetOpen in a new window

Other useful resources:
Telkom-Everynet Press ReleaseOpen in a new window

Murata-Everynet Press Release: please visit hereOpen in a new window.

Murata-Telkom webinar on-demand (*available in Bahasa Indonesia): please visit hereOpen in a new window.

To contact Telkom or Everynet:
Contact for TelkomOpen in a new window
Contact for everynetOpen in a new window

Contact

Please make inquiries about our solutions introduced here using the contact form below.


Partner Collaboration Solutions

End-to-End cellular IoT solution from Murata × ST × AVSystem

Leveraging on Murata’s LTE Cat-M1 and NB-IoT modules; STMicro's X-CUBE-CELLULAR SDK; and AVSystem's Anjay L2M2M Client SDK and Coiote IoT Device Management (DM) Platform, this end-to-end solution enables effortless and secure connection for your smart IoT devices.

Connectivity Solutions For NVIDIA🄬 JETSON™

Murata provides wireless connectivity solution to realize easy integration for NVDIA🄬 JETSON™ Nvidia's strong AI platform and Murata's wireless solution offer easy solution to achieve time to market.

Murata’s certified module on Everynet LoRaWAN® network operated by Telkom Indonesia change the dynamics of Industrial Revolution 4.0 to enable millions of connected IoT devices

Murata provides designers with a turn-key LoRaWAN® connectivity module solution to simplify and accelerate their IoT products development together with Everynet, a global leading LoRaWAN® network operator and Telkom Indonesia, the largest telecommunication and network provider in Indonesia, to enable the deployment of secure end-to-end solutions to address multiple applications in the smart cities, utilities, logistics and tracking, agriculture and many others.

Wi-Fi ® sensing for child presence detection(CPD)

Wi-Fi sensing can accurately detect breathing and motion anywhere inside the car without blind spots. Wi-Fi sensing can be freely located in contrast to cameras.

Murata’s Wi-Fi®/Bluetooth® and Cellular Cat-M1/NB-IoT AWS qualified modules enable cloud-connected IoT devices

Murata's qualified connectivity modules combining the excellence in module manufacturing with a large and diversified products portfolio, together with AWS cloud excellence powered by over 175 services and a dedicated IoT Core platform - providing scalability, security, analytics and device management services, accelerate and simplify the journey to develop IoT devices and end-to-end solutions.

Accelerating the AI & IOT solutions enriching our lives

Google combined Murata’s compact package technology and Google’s own Edge TPU chip enabling power-efficient and high-performance machine learning inference to create a new compact AI module.

VitaNet and Murata join forces to utilize Murata Bluetooth® module with QR code to convert industrial components to IoT

Cloud is enabled to directly control Bluetooth® device by reading QR code to identify a device. Authentication and secure Bluetooth® communication follow automatically.

Electric Imp IoT Connectivity Platform

Innovative platform which simply connects devices and the cloud

LPWA/Bluetooth® Low Energy Tag Linking Solution

"Condition" and "status" management solution utilizing LPWA

Integrated Wi-Fi+Bluetooth® MCU Modules

Integrated Wi-Fi, Bluetooth communication function and micro control unit in a single unit Easy to Use AT Command (Serial Communication)

Ayla IoT Platform

Ayla's end-to-end IoT software applications to provide secure and scalable connectivity, data analytics, and seamless user experiences. Ayla is solving the IoT so you don't have to.