muRata INNOVATOR IN ELECTRONICS

RFID solution

Global - English EMEA - English Global - English 日本語
MENU EMEA - English Global - English 日本語

Basic knowledge of RFID

What is RFID?

An image of reading RFID tags

RFID (radio frequency identification) is automatic recognition technology that uses wireless communication. Generally, a system or a part that uses an IC tag to identify or control various items via wireless communication is called RFID. Here, a description is given mainly of the features of RFID and the principle of wireless communication in order to provide basic knowledge concerning RFID.

Features

Data can be read at long distance

By using wireless communication, data can be read at distance of several meters. Data can be read from a tag that is in a high, relatively inaccessible place. Inventory count in a large store or a storehouse can be easily done while securing operators safety.

An image of reading RFID tags on packages from distanced area

Multiple tags can be read at once

RFID obviates the need to hold each item one by one in order to read the data. It enables the data in all of the tags to be read at once by simply passing the scanner over the tags. This greatly reduces the time required to carry out stocktaking, etc.

An image of reading RFID tag attached on cloths

Data can also be read from outside the box

Since data is communicated via radio waves, it can be read from outside the packing box without opening the box, even when a tag is attached to the product. Unlike barcode, which can not be read when the surface is damaged, RFID is highly immune to dirt, and can read data without problem even if the surface of the tag dirty.

An image of tags on products inside package

Long life

A passive type RFID tag can be used semi-permanently without a battery. In addition, because the tag contains a memory, the data can be re-written. Compared to barcode, RFID contains and exchanges the much larger amount of data.

An image of RFID tags

RFID for business improvement

Inventory management

RFID enables efficient Inventory count at logistics center, backyard, and storefront.

An image of RFID enables efficient Inventory count at logistics center, backyard, and storefront.

Search for goods

RFID improves the efficiency at in-coming and out-coming outgoing inspection in factory, logistics center, and stores.

An image of RFID improves the efficiency at in-coming and out-coming outgoing inspection in factory, logistics center, and stores.

In-coming and outgoing record

The recording operation can be quickly done just by going through gate-type reader/writer.

An image of the recording operation can be quickly done just by going through gate-type reader/writer.

Brand protection

RFID is a useful tool to prevent gray market and counterfeit products of luxury brands.

An image of RFID is a useful tool to prevent gray market and counterfeit products of luxury brands.

RFID frequency bands

RFID consists of four frequency bands, the LF band, HF band, UHF band, and microwave band. Among the four frequency bands, Murata’s RFID uses HF band and UHF band communication. Since international compatibility is guaranteed by the ISO/IEC 18000 series wireless communication standards. Our RFID products are used throughout the world.

LF band
The LF (Low Frequency) band employs an electromagnetic induction method, and has a long history of use compared to other communication bands. One of the example of application is wireless communication in a keyless entry system for an automobile. Although the read range is only several tens of centimeters, it is necessary to use a large number of windings on the antenna, making it difficult to fabricate a thin, compact antenna.
HF band
The HF (High Frequency) band exchanges data using an electromagnetic induction method. Compared to the LF band, the HF band requires much smaller number of windings on the antenna, making it easy to fabricate a thin, compact antenna. As the HF band uses 13.56 MHz, which is a frequency in the short wave band, the communication distance is relatively short. Therefore the HF band is suitable for applications in a proximity area, such as those in which persons and items are validated in a 1-to-1 ratio. An NFC (Near Field Communication) device, which is applied for electronic money such as transportation IC card, also uses HF band RFID.
UHF band
An electronics field type communication method is employed in the UHF (Ultra High-Frequency) band. The frequency range is between 860 and 960MHz, making the UHF band suitable for the applications that requires the communication distance of several meters to read multiple sets of data simultaneously. Most stock control and automatic inspection is carried out using this frequency band.
Microwave band
The microwave band uses the frequency of 2.45GHz, which belongs to the UHF band. Since this band includes the ISM band, which is also used by microwave ovens and wireless LAN (Wi-Fi), there are concerns about radio wave interference. It is therefore necessary to take preventive measures. Also the communication distance is only 2 to 3 meters which is much shorter than that of the band between 860 to 960 MHz.
Communication band LF HF/NFC UHF Microwave
Frequency to 135KHz 13.56MHz 860 to 960MHz 2.45GHz
Communication method Magnetic field communication Magnetic field communication Electronic field communication Electronic field communication
Communication range to 10cm to 10cm to several m to 3m
Directionality Wide Wide Medium Narrow
Effect of metal Medium Large Large Large
Effective of water Small Small Medium Large
Application examples Keyless entry Public type IC card, security control Stock control, asset management, etc

Principle of RFID communication

Please flick and have a look.

An image explaining principle of RFID communication.

Basically, RFID communication is performed when battery-free passive tag reflects carrier waves sent from the reader/writer.

Flow of communication

Contact us for inquiries and consultation

For customers looking for RFID tag/reader-writer.

Murata also offers hardwares from the lineup of RFID tag and reader-writer. Please find the detail in the product page.